Database export - Metasys - LIT-12013963 - Software Application - Mass Changes Tool - 3.0.0.x

Mass Changes Tool (MCT) Help

Product
Building Automation Systems > Configuration and Programming Tools > Mass Changes Tool
Document number
LIT-12013963
Version
3.0.0.x
Revision date
2022-06-24
The MCT can extract the contents of an archive database export file and edit the contents. The export file is always named with a .dbexport file extension. The following table outlines the file types that you can edit in the MCT.
Table 1. Archive database files
File type Description
archive.xml Contains the definition of the objects related to the selected device.
userDictionary.xml Contains the custom enumeration sets and the name of custom categories.
$site.UserTrees.xxxx.xml Contains the files related to single user views.