Custom enumeration sets - Metasys - LIT-12013963 - Software Application - Mass Changes Tool - 3.0.0.x

Mass Changes Tool (MCT) Help

Product
Building Automation Systems > Configuration and Programming Tools > Mass Changes Tool
Document number
LIT-12013963
Version
3.0.0.x
Revision date
2022-06-24

Menu Selection: Tools > Custom Enumeration Sets

You can use custom enumeration sets to add state texts both for binary and multistate objects. To add custom sets to standard sets, import the custom sets into the MCT. The site director device objects contain custom enumeration sets.

To load the custom enumeration sets, load the ZIP file exported from SCT, related to the site director device object.
Note: You can import one custom enumeration sets table at a time. To change the custom enumeration sets, reset the dictionary, and restart from the default condition.