Create BACnet EDE File - Metasys - LIT-12013963 - Software Application - Mass Changes Tool - 3.0.0.x

Mass Changes Tool (MCT) Help

Product
Building Automation Systems > Configuration and Programming Tools > Mass Changes Tool
Document number
LIT-12013963
Version
3.0.0.x
Revision date
2022-06-24

Menu Selection: Tools > Additional Functions > Create BACnet EDE File

The create BACnet EDE file function discovers BACnet devices on the network connected to a selected LAN card and creates an engineering data exchange file (CSV). You can use this file in the new file window to create an IMP file.
Note: To use this function, you must install and license the Multiprotocol Application eXplorer (MAX) software.