Overview - Metasys - LIT-12013963 - Software Application - Mass Changes Tool - 3.0.0.x

Mass Changes Tool (MCT) Help

Product
Building Automation Systems > Configuration and Programming Tools > Mass Changes Tool
Document number
LIT-12013963
Version
3.0.0.x
Revision date
2022-06-24
You can use Mass Changes Tool (MCT) to perform the following actions:
  • Edit the System Configuration Tool (SCT) database, with the SCT connectivity interface. Requires SCT 10.0 or later.
  • Edit the SCT export files (ZIP).
  • Edit the SCT dbexport files. Requires SCT 6.5 or later.
  • Generate the BACnet® EDE files in CSV format based on SCT export files (ZIP).
  • Generate the BACnet EDE files in CSV format based on SCT Database.
  • Generate MQTT Client configuration files (MCCF) for an SNx engine. Requires Metasys® 12.0 or later.
  • Generate IMP files for the SCT and engines.

The following table outlines the IMP files you can generate in the MCT.

Table 1. MCT IMP file generation
Generate IMP files for Related to Requires
SCT/NAE BACnet FEC/FAC controllers CAF files
SCT/NAE N2 Open FEC/FAC controllers CAF files
SCT/NAE BACnet FX controllers APD files
SCT/NAE N2 Open FX controllers APD files
SCT/NAE N2 DX9100 controllers DMO files
SCT/NAE N2 Open controllers PRN files
SCT/NAE N2 System 91 and N2 Open controllers NCM database DDL files
N30 database MPB files
Extended Data Engine database. Systems Integration Services Europe EDE files
SCT/NAE Systems Integration Services Europe Modbus® to BACnet Module Integration TXT files
SCT/NAE MIG devices drivers VCT files
SCT/NAE LON devices XIF files
SCT/NAE BACnet devices EDE files
SCT/NAE Extended Data Engine as BACnet device Systems Integration Services Europe EDE files
SCT/NIE5910 XL5K devices CSV files
SCT/NIE NIEx9 Modbus Integration VMD files
SCT/NIE NIEx9 M-Bus™ Integration M-Bus model files
SCT/NIE NIEx9 KNX™ Integration ESF files or KNXPROJ files
SCT/NIE NIEx9 Zettler™ Fire Integration TXT files
SCT/NIE NIEx9 Bosch™ Fire Integration DATA files
SCT/NIE NIEx9 SNMP (GET and SET) Integration SNR files
SCT/NIE89 OPC Servers DA Integration OPC auto discovery

The following table outlines the supported engines for integrations:

Table 2. Supported engines for integrations
Integration Supported engines Metasys version
Modbus NIEx9 Metasys 9.0.x or earlier
NCE25/NAE35/NAE45/NAE55/NAE85 Metasys 9.0.x/10.0 or later
SNE/SNC Metasys 10.1 or later
M-Bus NIEx9 Metasys 9.0.x or earlier
NCE25/NAE35/NAE45/NAE55/NAE85 Metasys 9.0.x/10.0 or later
SNE/SNC Metasys 10.1 or later
KNX NIEx9 Metasys 9.0.x or earlier
NCE25/NAE35/NAE45/NAE55/NAE85 Metasys 9.0.x/10.0 or later
SNE/SNC Metasys 10.1 or later
Zettler Fire NIEx9 Metasys 9.0.x or earlier
NAE55 Metasys 10.0 or later
SNE/SNC Metasys 10.1 or later
OPC UA™ NAE55/NAE85 Metasys 11.0 or later
SNE/SNC Metasys 11.0 or later
Victor-C•CURE™ NAE55/NAE85 Metasys 10.1 or later
SNE/SNC Metasys 10.1 or later
MQTT Client SNE/SNC Metasys 12.0 or later