Restore point - Metasys - LIT-12013963 - Software Application - Mass Changes Tool - 3.0.0.x

Mass Changes Tool (MCT) Help

Product
Building Automation Systems > Configuration and Programming Tools > Mass Changes Tool
Document number
LIT-12013963
Version
3.0.0.x
Revision date
2022-06-24

Menu Selection: File > Restore Point

The restore point feature provides the ability to return to a previous snapshot of the modified file. The restore point is automatically created when you perform one of the following actions:
  • Multiple paste
  • Update extensions name
  • Update field points name
  • Reset extensions unique ID
  • Propagate graphic reference
  • Paste from Excel®
  • Paste from clipboard
  • Paste on cells
  • Import CSV file for extensions
  • Import IMP file
  • Import new device
  • Table editor
  • Delete rows in the table
  • Convert alarm extensions to intrinsic alarming