New File - Metasys - LIT-12013963 - Software Application - Mass Changes Tool - 3.0.0.x

Mass Changes Tool (MCT) Help

Product
Building Automation Systems > Configuration and Programming Tools > Mass Changes Tool
Document number
LIT-12013963
Version
3.0.0.x
Revision date
2022-06-24

Menu Selection: File > New

You can use the New File - Type window to create IMP files for devices, controllers, and integrations. The steps to complete the creation of the file varies on the type of device, controller, or integration you select. For example, to create a file for a Modbus Integration, you need to specify the resource file that includes the details related to the points.
Figure 1. New File window