MQTT Client configuration user interface icons - Metasys - LIT-12013963 - Software Application - Mass Changes Tool - 3.0.0.x

Mass Changes Tool (MCT) Help

Product
Building Automation Systems > Configuration and Programming Tools > Mass Changes Tool
Document number
LIT-12013963
Version
3.0.0.x
Revision date
2022-06-24

The following table outlines the user interface icons in the broker definition tab.

Table 1. Broker definition icons
Icon Name Description
Add Adds a new broker definition to configure.
Delete Deletes a broker definition from the broker definition list.
Cancel Cancels current changes made to the broker definition properties.
Save Saves changes to the broker definition properties.
Refresh Refreshes the broker definition list.

The following table outlines the icons in the topic definition tab.

Table 2. Topic definition icons
Icon Name Description
Add Adds a new topic definition to configure.
Delete Deletes a topic definition from the topic definition list.
Cancel Cancels current changes made to the topic definition properties.
Save Saves changes to the topic definition properties.
Refresh Refreshes the topic definition list.
Export Exports a selected topic definition from the topic definition list as an Excel file.
Import Imports a topic definition in Excel file format into the topic definition list.

The following table outlines the user interface icons found in the point/payload definition tab.

Table 3. Point/payload definition icons
Icon Name Description
Add Topic Data-Tree Adds a new topic data-tree root.
Add Topic Sub-Path Adds a new top sub-path to a topic data-tree root.
Add Topic Sub-Paths Template Opens the topic sub-paths template window.
Delete Deletes a selected broker or topic definition.
Move Up Moves up a topic data-tree root or topic point in the topic treeview.
Move Down Moves down a topic data-tree root or topic point in the topic treeview.
Save Saves changes to a broker definition, topic definition, or point/payload definition.
Cancel Cancels current changes to a broker definition, topic definition, or point/payload definition.
Refresh Refreshes the topic definition list.
Export Exports selected topic sub-paths from the topic treeview as an Excel file.
Import Imports a topic sub-paths in Excel file format into the topic treeview.
Add Payload Object Adds an object to a custom payload.
Add Payload Element Adds an element to a custom payload.