MQTT Client configuration libraries - Metasys - LIT-12013963 - Software Application - Mass Changes Tool - 3.0.0.x

Mass Changes Tool (MCT) Help

Product
Building Automation Systems > Configuration and Programming Tools > Mass Changes Tool
Document type
User Guide
Document number
LIT-12013963
Version
3.0.0.x
Revision date
2022-06-24

Menu Selection: Tools > Additional Functions > MQTT Client Configuration Libraries

The MQTT Client configuration libraries provide the predefined broker, topic, and payload definitions. You can use the predefined definitions when you create a MQTT Client configuration file. You can create new definitions or edit the predefined definitions. The following figure shows an example of a predefined broker definition.
Figure 1. Broker definition library