Before you begin
Create and store the network engine database in
SCT before you start the MCT.
Procedure
-
Launch MCT.
-
Click ,
-
From the New File - Type window, select the MQTT Client Configuration icon, and click Finish.
-
To connect to the SCT Archive, enter the server name, user
name, and password.
-
Click Connect.
-
Select the Archive and Network Engine you want to use, and
click Next.
Note: The Devices tree
displays Metasys version 12 or later supported engines. To view engines at
Metasys Release 11.0 and earlier, select the Show
All Versions check box. Do not select an unsupported
engine.
-
Optional: In the Enter Configuration file info window, modify the
following fields:
-
Configuration Name
-
Configuration Description
-
Configuration File Name
-
Note
-
Click OK.