Creating a new file for a Modbus Integration - Metasys - LIT-12013963 - Software Application - Mass Changes Tool - 3.0.0.x
Mass Changes Tool (MCT) Help
- Product
- Building Automation Systems > Configuration and Programming Tools > Mass Changes Tool
- Document number
- LIT-12013963
- Version
- 3.0.0.x
- Revision date
- 2022-06-24
Procedure
-
Click .
-
In the New File - Type window, select the Modbus Integration icon, and click Next.
-
Click the Resource File ellipses and browse to your VMD resource file.
-
Click Open.
-
In the Unique ID field, enter a unique ID for your
device.
-
In the Name field, enter a name for your device.
-
In the Description field, enter a description for your
device.
-
From the Vendor Configuration
Data pane, in parameter [8], enter your branch name.
-
Click Next.
-
Optional: In the New File - Points window, you can modify the
information related to points. The VMD resource file automatically fills the
information displayed, except for the definitions of the units.
-
Optional: To add a unit definition to a
point, select the unit definition from the Unit drop-down list.
-
Click Next.
-
To add points to your device, click the >> icon.
-
Click Finish.