Exporting CSV file for extensions - Metasys - LIT-12013963 - Software Application - Mass Changes Tool - 3.0.0.x

Mass Changes Tool (MCT) Help

Product
Building Automation Systems > Configuration and Programming Tools > Mass Changes Tool
Document number
LIT-12013963
Version
3.0.0.x
Revision date
2022-06-24

About this task

The export function creates a preconfigured file for trend extensions. If the object already has trend extensions, the action column is given the M value. If the object has no trend extensions, the action column is given the A value.

Procedure

  1. Navigate to File > Export > Export CSV File for Extensions.
  2. Choose a location for the export file.
  3. In the File name field, enter a name for the export file.
  4. Click Save.