CSV values - Metasys - LIT-12013963 - Software Application - Mass Changes Tool - 3.0.0.x

Mass Changes Tool (MCT) Help

Product
Building Automation Systems > Configuration and Programming Tools > Mass Changes Tool
Document number
LIT-12013963
Version
3.0.0.x
Revision date
2022-06-24

Attributes require that you enter specific values. Numeric attributes require a floating point value. Integer or discrete attributes require an integer value. Boolean attributes require a T (true) value or a F (false) value. String attributes require a string value.

Values present in the cell of a column modify an existing extension or represent a parameter for a new extension. An empty cell applies no modification to the specified attribute. Cells with the value
<DEFAULT>
removes the attribute from the database and the SCT considers it as the default value.