Exporting selected points as an IMP file - Metasys - LIT-12013963 - Software Application - Mass Changes Tool - 3.0.0.x

Mass Changes Tool (MCT) Help

Product
Building Automation Systems > Configuration and Programming Tools > Mass Changes Tool
Document type
User Guide
Document number
LIT-12013963
Version
3.0.0.x
Revision date
2022-06-24

About this task

To export a subset of points in a field device node, complete the following steps:

Procedure

  1. From the All Items tree, select the node with the points that you want to export.
  2. Right-click the selected node, and click Export Selected Points as IMP file.
  3. In the Points Selection tree, select the points that you what to export.
  4. Click OK.
  5. Choose a location for the export file.
  6. In the File name field, enter a name for the export file.
  7. Click Save.