Exporting points as IMP file - Metasys - LIT-12013963 - Software Application - Mass Changes Tool - 3.0.0.x

Mass Changes Tool (MCT) Help

Product
Building Automation Systems > Configuration and Programming Tools > Mass Changes Tool
Document number
LIT-12013963
Version
3.0.0.x
Revision date
2022-06-24

About this task

To export all the points contained in a field device or trunk node, without the device object, complete the following steps:

Procedure

  1. From the All Items tree, select the node that you want to export.
  2. Right-click the selected node, and click Export Points as IMP file.
  3. Choose a location for the export file.
  4. In the File name field, enter a name for the export file.
  5. Click Save.