Copying and pasting multiple trend studies - Metasys - LIT-12013963 - Software Application - Mass Changes Tool - 3.0.0.x

Mass Changes Tool (MCT) Help

Product
Building Automation Systems > Configuration and Programming Tools > Mass Changes Tool
Document number
LIT-12013963
Version
3.0.0.x
Revision date
2022-06-24

About this task

To create multiple copies of a trend studies node, complete the following steps:

Procedure

  1. From the All Items tree, select the node that you want to copy.
  2. Right-click the selected node, and click Multiple Copy.
  3. Select the node under which you want to paste the copied node.
  4. Right-click the selected node, and click Multiple Paste.
  5. In the Base ID field, enter a unique object ID name and include the placeholder number character #.
  6. Optional: In the Name field, enter a name.
  7. In the Start field, enter the number you want for the start of the series.
  8. In the End field, enter the number you want for the end of the series.
  9. In the Step field, enter the number you want to increment the series.
  10. From the Format list, select the number format you want for the series.
  11. Click OK.
  12. In the Find field, enter the number you want to locate.
  13. In the Replace field, enter the new number.
  14. Click OK.