Convert alarm extensions as intrinsic alarming - Metasys - LIT-12013963 - Software Application - Mass Changes Tool - 3.0.0.x

Mass Changes Tool (MCT) Help

Product
Building Automation Systems > Configuration and Programming Tools > Mass Changes Tool
Document number
LIT-12013963
Version
3.0.0.x
Revision date
2022-06-24

Menu Selection: Right-click > Convert Alarm Extensions as Intrinsic Alarming

You can convert alarm extension objects into intrinsic alarm attributes of the parent object. This procedure is useful if you need to move from the Metasys native alarm management to fully compliant BACnet alarm management. This operation propagates to all children of the selected node. For example, if you select a trunk, all the extensions of points of all the devices belonging to the trunk are updated.