Changing the object type - Metasys - LIT-12013963 - Software Application - Mass Changes Tool - 3.0.0.x

Mass Changes Tool (MCT) Help

Product
Building Automation Systems > Configuration and Programming Tools > Mass Changes Tool
Document type
User Guide
Document number
LIT-12013963
Version
3.0.0.x
Revision date
2022-06-24

Procedure

  1. From the All Items tree, select the object.
  2. Right-click the selected object, and click Change Object Type.
  3. From Object Type list, select the new object type.
    Note: Unsupported attributes of the new object type, or attributes of a different type, for example relinquish default, are removed and set to default.
  4. Click OK.