Adding an extension to an object - Metasys - LIT-12013963 - Software Application - Mass Changes Tool - 3.0.0.x

Mass Changes Tool (MCT) Help

Product
Building Automation Systems > Configuration and Programming Tools > Mass Changes Tool
Document number
LIT-12013963
Version
3.0.0.x
Revision date
2022-06-24

Procedure

  1. From the All Items tree, select the object.
  2. Right-click the selected object, and click Add Extension.
  3. From the Attribute list, select the extension type.
  4. From the Object Type list, select the object type.
  5. In the Unique ID field, enter a unique object ID.
  6. Optional: In the Name field, enter a new name.
    Note: Configure the default Unique ID and Name in the default values section in the settings menu.
  7. Click OK.