Procedure
- From the All Items tree, select the object.
- Right-click the selected object, and click Add Extension.
- From the Attribute list, select the extension type.
- From the Object Type list, select the object type.
- In the Unique ID field, enter a unique object ID.
-
Optional: In the Name field, enter a new
name.
Note: Configure the default Unique ID and Name in the default values section in the settings menu.
- Click OK.