The SA bus connects IOMs, XPMs , VSDs, and NS-Series network sensors to equipment controllers. Figure 1 in End-of-Line termination on SA Bus shows three SA bus examples. Table 1 provides SA Bus rules and limits. Table 2 provides SA Bus specifications.
Category |
Rules/limits |
---|---|
General |
Each bus supervisor supports one SA Bus (and each SA Bus is a single segment). |
Number of devices supported on the SA Bus |
The guideline for the maximum total number of devices supported on an SA Bus is 10. The SA bus supervisor provides power for all subordinate devices connected to the SA bus, including up to eight NS network sensors. IOMs and XPMs connected to the SA bus are not powered by the bus supervisor. |
SA Buses do not support repeaters. See Table 1 for SA Bus power consumption. |
|
Cable length |
365 m (1,200 ft) maximum bus length |
152 m (500 ft) maximum distance between an NS network sensor and the bus supervisor (CGM, CVM, FAC, FEC, or VMA supplying power to the sensor) using bus cable connected to the SA Bus screw terminal blocks |
|
30 m (100 ft) maximum length for network sensors using bus cables connected to the RJ-Style modular jack (6-Pin SA Bus Port) |
|
366 m (1,200 ft) maximum bus length |
|
Recommended cable type |
Screw Terminal Connections: 22 AWG Stranded 4-wire, 2-Twisted Pairs, Shielded Cable for screw terminals. Modular Jack Connections: 6-Pin RJ-Style Modular Connectors with 24 or 26 AWG Solid 6-Wire, 3 Twisted-Pairs |
EOL termination |
Each SA bus supervisor has integral (fixed ON) EOL termination, which typically provides sufficient EOL termination on an SA bus. Long SA bus runs or persistent communication problems on an SA bus may require EOL termination at the last device on the SA bus (in addition to the integral EOL termination at the SA bus supervisor). |
Mixing device types |
Do not mix RJ-style modular (phone) jack devices and screw terminal devices on the SA bus. |
Category | Specification |
---|---|
Error checking | Message Headers checked using 8-bit CRC test. Message data check using 16-bit CRC test. |
Device addressing | 0-255 (See Device addressing on the MS/TP Bus for more information.) |
Data transmission standard | RS485 |
Signaling method | BACnet® MS/TP |
Signaling rate | 9600; 19,200; 38,400 (default); or 76,800 baud as selected by the bus supervisor |
Transient immunity | Meets EN61000-4-4 and EN6100-4-5 requirements for heavy industrial applications. Protected against misapplication of 24 VAC. |
Shield grounding | One hard ground per bus segment when using shielded cable |
Physical configuration | Daisy-chained (screw terminal only). |