BACnet Router Wiring - Metasys - LIT-12011034 - General System Information - Metasys System - Release 11.0

MS/TP Communications Bus Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011034
Version
Release 11.0
Revision date
2022-02-07
Language
English

Figure 1 shows how to wire the BACnet Router to the Metasys system. This example features the Loytec Router, Model LIP-ME201C, the recommended device from Loytec Electronics GmbH.

Figure 1. Wiring BACnet Router

Note: Configure the BACnet Router before you connect it to the building network. If the BACnet Router is commissioned using the IP, use an Ethernet patch cable. Terminal 1 on the router is for the reference wire. Not all devices use the same markings.