The FC bus requires EOL termination at the end of each bus segment. Figure 1 shows four examples of EOL termination on the FC bus.
Figure 1. FC Bus segment EOL termination scenarios
Scenario | Description |
---|---|
1 | FC Bus with an SNE at the end of the line |
2 | FC Bus with an SNE not at the end of the line |
3 | FC Bus in two segments with the repeater at the end of both segments |
4 | FC Bus in two segments with the repeater not at the end of both segments |