For most devices on an MS/TP bus, the (non-supervisory) device address is set by positioning the Rotary or DIP switches on the device’s address DIP switch block. The DIP switch blocks are binary switch blocks, with each switch representing a binary numerical value when the switch is in the ON position. The CGM and CVM controllers have three rotary switches for setting the device address.
The device address set on the address DIP switch block or rotary switches applies to the device connection on the bus where the device is not the bus supervisor. For example, the rotary switches on CGMs or CVMs and the DIP switches on FACs, FECs, or VMAs (manager devices) set the device address for the device connection to the FC bus (or Remote Field Bus). If the CGM, CVM, FAC, FEC or VMA also supervise an SA bus, the controller's address on an SA bus is 0 by default (Figure 1).
An IOM or XPM has only one device connection, which can connect to either an FC bus or an SA bus (but not both); therefore, the device address set on an IOM or XPM applies to the bus to which the IOM is connected. (An IOM or XPM is never a bus supervisor.)
Address value/ Address range |
Class |
Devices |
---|---|---|
0 |
Bus Supervisor |
FC Bus: NAE, NCE, SNE, or SNC SA Bus: NCE, SNC, CGM, CVM, CGE, CVE, FAC, FEC, or VMA Remote Field Bus: BACnet Router C4-CGMs, C4-CVMs, CH-PCA, CH-PCG, or CH-PCV |
1 |
Reserved for JCI use |
Reserved for the Field Inspection Tool (FIT) |
2 |
Reserved for JCI use |
Reserved for Mobile Access Portal (MAP) and ZFR/ZFRPro Wireless Field Bus Converter |
3 |
Reserved for JCI use |
DIS1710 Local Controller Display |
4–127 C4-CGMs, C4-CVMs, CH-PCA, |
Manager Range |
FC Bus: CGMs, CVMs, FACs, FECs, VMAs, IOMs, XPMs, and TECs.Remote Field Bus: CGMs, CVMs, FACs, FECs, VMAs, IOMs, XPMs and TECs. SA Bus: IOMs and XPMs
Note: On applications using an
NCE, the address value 4 is reserved for the NCE’s integral
field controller. On applications using ZFR1810
coordinators, address values 120 to 127 are reserved for
multiple coordinators.
|
128–254 |
Subordinate Range |
Subordinate devices, VSDs, and NS network sensors on the SA Bus. Not Supported on the FC bus. |
198 |
Reserved |
VAV Balancing Sensor (handheld) |
199 |
Reserved |
Most NS Series Network Sensor models or VAV Balancing Sensor (wall-mounted) |
200–219 |
Reserved |
NS Series Network Sensors |
255 |
Broadcast |
Do not apply address 255 to any device. |
As you set the device address on controllers with dip switch blocks, the best practice is to set the highest switch value first, then the next highest switch value, and so on, until the total of the switch values equal the intended device address. For example, positioning switches 16, 4, and 1 to ON sets the device address to 21 for a device on the FC bus.
Notes:
- You must set switch 128 to OFF on all Metasys field controllers that are hardwired to an FC bus. Set switch 128 to ON only on FACs, FECs, VMAs, and IOMs that operate on a Metasys ZFR Series Wireless Field Bus.
- Devices may go offline momentarily when a device address is changed on an active bus. A device reset is not required on equipment controllers or supervisory engines after changing the MS/TP address.
Some devices, such as the TEC36xx Series thermostats and third-party MS/TP devices, use their own configuration settings to establish the device address for their connection to the bus. Drilling down through menus in software configures the addresses of the NS8000 graphical display model and the TEC3000 series. Refer to the device manufacturer’s product documentation for instructions on setting the device address. The device address values for TEC thermostats and all third-party devices must comply with the rules and ranges described previously.
Rotary switch dials
The SNC has 3 rotary switch dials labeled Controller Number for setting the controller number, which can be numbered from 000 to 999. The switches are shipped from the factory set to 000. You can use them to set a decimal number from 000 to 999 as a unique identifier for each SNC. The numbers are ordered from left to right, most significant bit (MSB) to least significant bit (LSB) when the controller is oriented as shown in the following figure where the switches are set to 1 2 3 (controller address 123).