Commission the devices on the MS/TP bus using the CCT software. Refer to the Controller Tool Help (LIT-12011147) for information on commissioning an MS/TP bus application.
Commission the devices on the local and remote MS/TP buses with the CCT software using either the Mobile Access Portal (MAP) Gateway or in passthrough mode when connected to an NAE, NCE, SNC or SNE. Refer to Controller Tool Help (LIT-12011147) for information on commissioning an MS/TP bus application.
Hardware points can be auto discovered from the online UI of the NAE, the Application and Data Server (ADS), the Extended Application and Data Server (ADX), or the Open Data Server (ODS) .