Configuring repeaters - Metasys - LIT-12011034 - General System Information - Metasys System - Release 11.0

MS/TP Communications Bus Technical Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Technical Bulletin
Document number
LIT-12011034
Version
Release 11.0
Revision date
2022-02-07
Language
English

The instructions for configuring the repeater for use with the FC bus require that you perform the following:

  • Set the baud rate to match the FC bus baud rate.

  • Wire the repeater between two segments of the MS/TP bus. If you are using this repeater in a branch, the side with the branch has double the number of wires terminated. See Figure 1.

  • Set the EOL jumpers on the repeater according to Table 1.

Note: The EOL jumpers are located below the cover of the repeater.
Note: Sides A and B have separate EOL settings. Determine the settings individually.

For repeater installation instructions and important safety information, refer to the repeater manufacturer’s literature.

WARNING
  • Risk of Electric Shock:
  • Disconnect or isolate all power supplies before making electrical connections. More than one disconnection or isolation may be required to completely de-energize equipment. Contact with components carrying hazardous voltage can cause electric shock and may result in severe personal injury or death.
Table 1. EOL settings for repeater

Side

Jumper

Instructions

Side A

J1 and J2

At end-of-line: Install both jumpers over Pins 1 and 2 (EOL In).

Not at end-of-line: Install both jumpers over Pins 2 and 3 (EOL Out).

Side B

J3 and J4

At end-of-line: Install both jumpers over Pins 1 and 2 (EOL In).

Not at end-of-line: Install both jumpers over Pins 2 and 3 (EOL Out).

Figure 1. Configuring the repeater