To set the modem with the end-of-line selection set to Out, wire the 9-pin connector using solder connections as in Figure 1.
Note: The following figure shows the 9-pin female connector. The pin numbers on the
9-pin male connector are reversed.
Figure 1. Female modem cable connector: EOL set to Out

FC Bus signal |
For EOL selection |
For non-EOL selection |
---|---|---|
FC + |
Terminal 7, Jumper 7-3 |
Terminal 3 |
FC - |
Terminal 8, Jumper 8-9 |
Terminal 9 |
REF |
Terminal 1 or 5 |
Terminal 1 or 5 |
SHIELD |
Tape Back |
Tape Back |