Setting termination on fiber modems - Metasys - LIT-12011034 - General System Information - Metasys System - Release 11.0

MS/TP Communications Bus Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Technical Bulletin
Document number
LIT-12011034
Version
Release 11.0
Revision date
2022-02-07
The 2110BAC modem does not have an EOL jumper. Instead, establish EOL termination on a 2110BAC modem by properly terminating the FC bus wires to the 9-pin connector. Soldering the wires to specific pins and soldering two jumper wires configures the modem as an end-of-line device (see Figure 1, Figure 1, and Table 1 for more information).
Note: A DIN rail mounting version of the Model 2110BAC may be available as Model 2110BAC-DIN. This model would not require soldering the MS/TP wires. However it does not appear on the S.I. Tech web site at the time of this writing. Contact S.I. Tech using contact information on their web site at http://www.sitech-bitdriver.com/index.htm.

Do not set the fiber modem as an EOL device on the SA bus.