Connect the MS/TP bus to the 2110BAC modem by soldering the MS/TP wires to pins on the 9-pin connector, which can also configure the modem as an EOL device. To connect the bus, see Setting termination on fiber modems.
Note: A DIN rail mounting version of the Model 2110BAC may be available as Model
2110BAC-DIN. This model would not require soldering the MS/TP wires. However, Model
2110BAC-DIN does not appear on the S.I. Tech web site at the time of this writing.
Contact S.I. Tech using contact information on their web site at http://www.sitech-bitdriver.com/index.htm.