Fiber-optic modems - Metasys - LIT-12011034 - General System Information - Metasys System - Release 11.0

MS/TP Communications Bus Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Technical Bulletin
Document number
LIT-12011034
Version
Release 11.0
Revision date
2022-02-07

You can install the 2110BAC fiber-optic modems in any location on the FC bus. Just as only two repeaters can be cascaded on the FC bus, only two pairs of 2110BAC modems can be cascaded.

The first installation step is to route the optical fiber and connect each modem to the ends of the fiber. The second step is to connect the FC bus on both sides of the modems.