Report Menu - Metasys - LIT-12012443 - Software Application - MS-FIT100-0 Field Inspection Tool

MS-FIT100-0 Field Inspection Tool User Guide

Product
Accessories > Field Inspection Tool > MS-FIT100-0 Field Inspection Tool
Document number
LIT-12012443
Revision date
2019-09-11

The FIT can save up to seven reports. The information saved to a report is captured from the current data in the FIT’s memory. Normally only complete and functional FC Bus installations are saved to Reports but if problems persist during installation validation a Report could be used to capture and share information about a bus or bus segment.

Each Report has three types of information stored as follows:

  • General Bus Information
  • Device Information
  • Issue Information