The General information section of the report is one record and contains the following information:
| Heading | Description |
|---|---|
| Report Name | Name of the report entered by the user. |
| Health | The Bus Health Index. |
| Devices | The quantity of devices on the bus. |
| Idle Volts | Differential Voltage Idle. This is + to – voltage reading without communication. |
| Idle + | + to Com Idle Voltage reading without communication. |
| Idle - | - to Com Idle Voltage reading without communication. |
| Issues | The number of issues reported. |
| Token Loop ms | The recorded Loop Time. |
| Runtime sec | This is the number of seconds from when the FIT was powered on until the data was captured. The FIT does not have a Clock. If report date and time is desired the information must be captured manually. |
| Report # (Seq Num) | This is a sequential number the FIT assigns to each report. |