The Device information section of the report is one record per address discovered. Some information in this section can only be completed if:
- a ScanBus was performed
- The device is a Johnson Controls manufactured product.
If either of these two items are not true the report fields, except Address, will result with unknown. See Table 4 for information on the Device Section.
Heading | Description |
---|---|
Address | The device address for each device recorded. By default these are sorted ascending by address number. |
Model | Device object Model Name property for device at address. (Typically only Johnson Controls manufactured devices.) |
Type | Device object Vendor property for device at address. (Typically only Johnson Controls manufactured devices.) |
Transmit Volts | The differential communication voltage recorded for the device at address. |
EOL | The Position of the End-Of-Line Switch reported at address. (Typically only Johnson Controls manufactured devices.) |