FIT User Guidelines - Metasys - LIT-12012443 - Software Application - MS-FIT100-0 Field Inspection Tool

MS-FIT100-0 Field Inspection Tool User Guide

Product
Accessories > Field Inspection Tool > MS-FIT100-0 Field Inspection Tool
Document number
LIT-12012443
Revision date
2019-09-11

Observe the following guidelines when using the FIT:

  • Do not use the RJ-12 cable to support the weight of the FIT. The FIT comes with a magnetic strap for hanging from ductwork or other metal surfaces.
  • Keep the FIT in the protective shell with which it ships.
  • The FIT has not been designed for prolonged outdoor use. Leaving it in outdoor environments may result in damage.
  • Keep FIT power off when not in use. Test the FIT batteries and replace them when necessary. Prolonged battery use may cause battery leakage to occur.

To view training videos on using the FIT tool, click here to visit the uLearn website.