Type of field device |
Type of Input/Output |
Termination diagrams |
---|---|---|
Temperature Sensor |
UI |
|
Voltage Input - External Source |
UI |
|
Voltage Input - Internal Source |
UI |
|
Voltage Input (Self-Powered) |
UI |
|
Current Input - External Source (Isolated) |
UI |
|
Current Input - Internal Source (2-wire) |
UI |
|
Current Input - Internal Source (3 wire) |
UI |
|
Current Input - External Source (in Loop) |
UI |
|
Feedback from EPP-1000 |
UI |
|
Dry Contact (Binary Input) |
UI or BI |
|
0–10 VDC Output to Actuator (External Source) |
AO |
|
0–10 VDC Output to Actuator (Internal Source) |
AO |
|
Current Output |
AO |
|
24 VAC Triac Output (Switch Low, External Source) |
AO |
|
Analog Output (Current) |
AO |
|
4–20 mA Output to Actuator |
AO |
|
4–20 mA Output to Actuator |
AO |
|
Incremental Control to Actuator (Switch Low,
Externally Sourced)
|
BO |
|
24 VAC Binary Output (Switch Low, Externally
Sourced)
|
BO |
|
24 VAC Binary Output (Switch High, Externally
Sourced)
|
BO |
|
Incremental Control to Actuator (Switch High,
Externally Sourced)
|
BO |
|
Network Stat with Phone Jack (Fixed Address = 199) |
SA Bus |
Note: The bottom jack (J2) on the TE-700 and TE-6x00
Series Sensors is not usable as a zone bus or an SAB connection.
|
Network Stat with Terminals Addressable |
SA Bus |
|
Network Stat with Terminals (Fixed Address = 199) |
SA Bus |
|
A set of Johnson Controls termination diagrams
provides details for wiring inputs and outputs to the expansion modules. See the figures
in this section for the applicable termination diagrams.
Note: References to the analog
output apply to the XPM09090 model only.