Input and Output terminal blocks - Metasys - M4-XPM04060 - M4-XPM09090 - M4-XPM18000 - Field Device - M4-XPM Expansion Module - 13.0

M4-XPM Expansion Modules Installation Guide

Product
Controls > Expansion Modules > M4-XPM Expansion Module
Document type
Installation Guide
Document revision
C
Version
13.0
Revision date
2023-10-02
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10143-02147

XPM models have removable input and output terminal blocks. On XPM09090 and XPM04060 models, all of the input terminal blocks are located on the bottom of the controller, and the output terminal blocks are located on the top of the expansion module. The XPM18000 has inputs only which are located on both the top and bottom of the expansion module. For information about removing a terminal block, see Removing a terminal block. For more information about I/O terminal functions, requirements, and ratings, see Terminal wiring guidelines, functions, ratings, and requirements.