Wiring - Metasys - M4-XPM18000 - M4-XPM09090 - M4-XPM04060 - Field Device - M4-XPM Expansion Module - 13.0

M4-XPM Expansion Modules Installation Guide

Product
Controls > Expansion Modules > M4-XPM Expansion Module
Document type
Installation Guide
Document revision
C
Version
13.0
Revision date
2023-10-02
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10143-02147

Observe the following guidelines when wiring an XPM expansion module:

CAUTION
  • Risk of Electric Shock:
  • Disconnect the power supply before making electrical connections to avoid electric shock.
ATTENTION
  • Mise En Garde: Risque de décharge électrique:
  • Débrancher l'alimentation avant de réaliser tout raccordement électrique afin d'éviter tout risque de décharge électrique.
CAUTION
  • Risk of Property Damage:
  • Do not apply power to the system before checking all wiring connections. Short circuited or improperly connected wires may result in permanent damage to the equipment.
ATTENTION
  • Mise En Garde: Risque de dégâts matériels:
  • Ne pas mettre le système sous tension avant d'avoir vérifié tous les raccords de câblage. Des fils formant un court-circuit ou connectés de façon incorrecte risquent d'endommager irrémédiablement l'équipement.
Important: Do not exceed the expansion module electrical ratings. Exceeding the electrical ratings can result in permanent damage to the expansion module and void any warranty.
Important: Use copper conductors only. Make all wiring in accordance with local, national, and regional regulations.
Important: Electrostatic discharge can damage expansion module components. Use proper electrostatic discharge precautions during installation, setup, and servicing to avoid damaging the expansion module.

For detailed information about configuring and wiring an MS/TP Bus, FC bus, and SA bus, refer to the MS/TP Communications Bus Technical Bulletin (LIT-12011034) .