Troubleshooting expansion modules - Metasys - M4-XPM18000 - M4-XPM09090 - M4-XPM04060 - Field Device - M4-XPM Expansion Module - 13.0

M4-XPM Expansion Modules Installation Guide

Product
Controls > Expansion Modules > M4-XPM Expansion Module
Document revision
C
Version
13.0
Revision date
2023-10-02
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10143-02147

Observe the Status LEDs on the front of the expansion module. Table 1 provides LED status indicator information for troubleshooting the expansion module. To troubleshoot a local controller display, refer to the DIS1710 Local Controller Display Technical Bulletin (LIT-12011270) or Local Controller Display User Guide (LIT-12013762) .