Removing a terminal block - Metasys - M4-XPM04060 - M4-XPM09090 - M4-XPM18000 - Field Device - M4-XPM Expansion Module - 13.0

M4-XPM Expansion Modules Installation Guide

Brand
Metasys
Product name
M4-XPM Expansion Module
Document type
Installation Guide
Part number
24-10143-02147
Document revision
C
Version
13.0
Revision date
2023-10-02
Product status
Active
Language
English

About this task

To remove a terminal block from the circuit board, complete the following steps:

Note: You need a flat blade screwdriver to remove the terminal block.

Procedure

  1. To prevent any possibility of damage from an accidental short, remove power from the expansion module.
  2. Underneath the terminal block, in the small gap between the bottom of the terminal block and the circuit board, insert the flat blade of the screwdriver.
    Figure 1. Terminal block
  3. To detach the left-hand side of the terminal block, position the flat blade underneath the terminal block to the left, and push down the screwdriver handle. When you do this, you are using the screwdriver as a lever to pry up the terminal block.
  4. To detach the right-hand side of the terminal block, position the flat blade underneath the terminal block to the right, and push down the screwdriver handle.
  5. If necessary, repeat steps 3 and 4 until the terminal block is removed.