Configuring wireless communications - Metasys - M4-XPM04060 - M4-XPM09090 - M4-XPM18000 - Field Device - M4-XPM Expansion Module - 13.0

M4-XPM Expansion Modules Installation Guide

Brand
Metasys
Product name
M4-XPM Expansion Module
Document type
Installation Guide
Part number
24-10143-02147
Document revision
C
Version
13.0
Revision date
2023-10-02
Product status
Active
Language
English

About this task

To configure an expansion module for use with the ZFR183x Pro Series Wireless Field Bus system, complete the following steps:

Procedure

  1. Disconnect the 24 VAC supply from the expansion module.
  2. Wire the input/output terminals and FC bus.
    Note: In wireless network applications, do not connect any wires to the FC bus terminal block.
  3. Important: Before the XPM expansion module is powered on, connect the ZFR183x Pro Wireless Field Bus Router to the FC bus port (RJ-12 modular jack) on the front of the device.
  4. Ensure that the expansion module's rotary switches are set to the correct device address. For details about setting a device address, see Setting the device address.
  5. Reconnect the 24 VAC supply to the expansion module.

    For more information about the ZFR Pro Wireless Field Bus system, refer to the WRG1830/ZFR183x Pro Series Wireless Field Bus System Technical Bulletin (LIT-12013553).