Commissioning - Metasys - M4-XPM04060 - M4-XPM09090 - M4-XPM18000 - Field Device - M4-XPM Expansion Module - 13.0

M4-XPM Expansion Modules Installation Guide

Product
Controls > Expansion Modules > M4-XPM Expansion Module
Document type
Installation Guide
Document revision
C
Version
13.0
Revision date
2023-10-02
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10143-02147

You commission expansion modules with the Controller Configuration Tool (CCT) software using either Mobile Access Portal (MAP) Gateway, a ZFR wireless dongle, or in passthrough mode when connected to a Network Engine. Refer to the Controller Tool Help (LIT-12011147) for detailed information on commissioning expansion modules.