Wall mount applications - Metasys - M4-XPM04060 - M4-XPM09090 - M4-XPM18000 - Field Device - M4-XPM Expansion Module - 13.0

M4-XPM Expansion Modules Installation Guide

Product
Controls > Expansion Modules > M4-XPM Expansion Module
Document type
Installation Guide
Document revision
C
Version
13.0
Revision date
2023-10-02
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10143-02147

About this task

To mount a XPM expansion module directly on a wall or other flat vertical surface, complete the following steps:

Procedure

  1. Pull the two bottom mounting clips outward and ensure they are locked in the extended position.
  2. Determine the proper mounting position the expansion module will be installed. Mark the mounting hole locations on the wall using the dimensions for the expansion module listed in Mounting features and dimensions. Alternatively, hold the expansion module up to the wall or surface in a proper mount position and mark the hole locations through the mounting clips.
  3. Drill holes in the wall or surface at the marked locations, and insert appropriate wall anchors in the holes (if necessary).
  4. Hold the expansion module in place, and insert the screws through the mounting clips and into the holes (or anchors). Carefully tighten all of the screws.
    Important: Do not over-tighten the mounting screws. Over-tightening the screws may damage the mounting clips.