Mounting features and dimensions - Metasys - M4-XPM18000 - M4-XPM09090 - M4-XPM04060 - Field Device - M4-XPM Expansion Module - 13.0

M4-XPM Expansion Modules Installation Guide

Product
Controls > Expansion Modules > M4-XPM Expansion Module
Document revision
C
Version
13.0
Revision date
2023-10-02
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10143-02147
Figure 1. Back of XPM04060 and XPM18000 expansion module
Figure 2. Back of XPM09090 expansion module
Note:
  • Mounting dimensions are listed in millimeters in the above figures.
  • The DIN rail channel and the mounting clips are shown in an extended position.