DIN rail mount applications - Metasys - M4-XPM18000 - M4-XPM09090 - M4-XPM04060 - Field Device - M4-XPM Expansion Module - 13.0

M4-XPM Expansion Modules Installation Guide

Product
Controls > Expansion Modules > M4-XPM Expansion Module
Document revision
C
Version
13.0
Revision date
2023-10-02
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10143-02147

About this task

To mount a XPM expansion module horizontally on a 35 mm DIN rail (recommended method), complete the following steps:

Procedure

  1. Securely mount a 20 cm (8 in.) or longer section of 35 mm DIN rail horizontal and centered in the desired space so that the expansion module mounts in the horizontal position.
  2. Pull the two bottom mounting clips outward from the expansion module to the extended position (Figure 1).
  3. Hang the expansion module on the DIN rail by the hooks at the top of the (DIN rail) channel on the back of the expansion module (Figure 1), and position the expansion module snugly against the DIN rail.
  4. Push the bottom mounting clips inward (up) to secure the expansion module on the DIN rail.
  5. To remove the expansion module from the DIN rail, pull the bottom mounting clips out to the extended position and carefully lift the expansion module off the DIN rail.