Installation - Metasys - M4-XPM18000 - M4-XPM09090 - M4-XPM04060 - Field Device - M4-XPM Expansion Module - 13.0

M4-XPM Expansion Modules Installation Guide

Product
Controls > Expansion Modules > M4-XPM Expansion Module
Document type
Installation Guide
Document revision
C
Version
13.0
Revision date
2023-10-02
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10143-02147

Observe the following guidelines when installing an XPM expansion module:

  • To minimize vibration and shock damage transport the expansion module in the original container.

  • Verify that all parts shipped with the expansion module.

  • Do not drop the expansion module or subject it to physical shock.