Method for tightening terminal blocks - Metasys - M4-SNE10502-0 - M4-SNE22002-0 - M4-SNE110L2-0 - M4-SNE11002-0 - Supervisory Device - Network Engine - 16.0

M4-SNE Installation Guide

Product
Document revision
N
Version
16.0
Revision date
2026-06-03
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10143-01647

Important: Remove power from the controller before beginning this procedure. Failure to de-energize the controller can result in equipment damage.
Important: It is best practice to remove the terminal block from the pin headers on the unit before wiring the terminal blocks.

Do not use more force than is necessary when tightening the terminal block screws. To prevent applying excessive force when tightening the screws, apply the following steps:

  1. Tighten the terminal screws until the screw is snug on the wire, and then tighten the screw an additional quarter (90°) to half (180°) turn.
  2. Only use enough downward force necessary to keep the screwdriver bit engaged with the screw. Too much downward force while tightening the terminal screws can damage the terminal.

    If a terminal block exhibits any symptoms of damage, replace the terminal block. For detailed information about replacing terminal blocks, refer to the Terminal Block Retrofit Installation Guide (LIT-12014622). See the following table for replacement terminal block kits:

    Table 1. Terminal block replacement part numbers
    Product code number Description
    ACC-TBKPWFCSA-1 Power, FC Bus, and SA Bus terminal block replacement kit for SNE, CG series, CV series, CC series, and XPM products. Kit includes 5 of each terminal block type. 15 terminal blocks in total. Power is grey, SA Bus is orange, FC Bus is blue, and all are unnumbered.