The SNx supports a second, non-routable Ethernet network through a USB-to-Ethernet adapter (ACC-USBETH-0). You must connect the adapter between the SNx’s USB port and a second Ethernet network. This external Ethernet network must be limited to a single subnet and be physically separated from the internal Ethernet network to prevent communication between the two networks.
Important: Do not attempt to configure the External LAN and
External LAN IP Data Link if the USB-to-Ethernet adapter is not plugged in to the
engine. Figure 1 shows the External LAN
property that should remain OFF and Figure 2 shows the External LAN IP
Communication Mode that should remain as None until after the
USB-to-Ethernet adapter is connected.
Figure 1. External LAN property in the Metasys UI Focus tab
Figure 2. External LAN IP Communication Mode in the Metasys UI Network tab
After you complete installation and wiring, refer to the
SNE Commissioning Guide (LIT-12013352)
for information about
configuration.