The SNE connects to Modbus RTU devices in three different ways:
- Option 1: Modbus connected to the FC Bus terminals.
- Option 2: Modbus connected to USB through the USB-to-RS-485 adapter, if the FC Bus is unavailable. The SNx engines include built-in RS-485 ports which are primarily intended for legacy N2 or BACnet MS/TP protocols. If these protocols are in use and you do not have an RS-485 port available for other third-party integration devices, use a USB-to-RS-485 adapter to connect third-party integration devices.
- Option 3: Modbus connected to USB through the USB-to-RS-232 adapter. Use this option if a single third-party device is connected and requires RS-232 connection.