The SNE can connect to the M-Bus network devices by using the USB-to-M-Bus adapter. Two components are needed: USB cable (Type B) and the M-Bus Mikro-Master USB device, or the ACC-USBMBUS-0. After installation and wiring are complete, refer to the Network Engine and Server Commissioning for M‑Bus Vendor Integration Application Note (LIT-12013149) for additional information.