Connecting LonWorks devices - Metasys - M4-SNE10502-0 - M4-SNE22002-0 - M4-SNE110L2-0 - M4-SNE11002-0 - Supervisory Device - Network Engine - 16.0

M4-SNE Installation Guide

Product
Document revision
N
Version
16.0
Revision date
2026-06-03
Product status
Active
docpartnumberlabel
Part No.
Part number
24-10143-01647

The SNE connects to LonWorks network devices through a USB-to-LON adapter (code number ACC-USBLON-0) that is wired between the USB port and the LON network. After installation and wiring are complete, refer to the LonWorks Network Integration with NAE and LCS Technical Bulletin (LIT-1201668) for additional information.

  1. Connect the 2-wire cable from the LonWorks network trunk to the removable 3-pin terminal block on the USB-to-LON adapter (code number ACC-USBLON-0) as shown in Figure 1. The SHD connection is not used. Connect the USB cable from the USB adapter to the USB-1 or USB-2 port on the SNE. You can use either port.
    Important: Use only the USB adapters that were tested and qualified for use with the SNE. Other non-qualified adapters do not function in the USB ports of the SNE. See USB ports for more information.
    Figure 1. LonWorks Network terminal block and wiring connections
    Callout Description
    1 USB connection (to USB-1 or USB-2)
    2 LonWorks terminal block; wires are not polarity sensitive
    3 Optional shield; connect shields together and insulate with tape
  2. Go to Connecting the power source.