The SNE connects to a KNX network device by using
the KNX/IP interface router. After installation and wiring are complete, refer to the
Network Engine and Server Commissioning for KNX Vendor Integration
Application Note (LIT-12013148)
for additional
information.
-
Connect an Ethernet cable to the port on the front of the KNX gateway as shown
in Figure 1.
Note: Depending on the size of your network, you can use either a KNX Interface
or Router as a gateway. The Interface connects the network engine to a
single KNX line, while the Router acts as both an Interface and a Line
Coupler over Ethernet to connect the network engine to the network, not to a
single device.
Figure 1. KNX/IP Interface Router
| Callout |
Description |
| 1 |
To power supply |
| 2 |
To KNX devices |
| 3 |
To Ethernet network |
-
For a single KNX line, wire from the red and black terminals on the gateway to
the devices. For multiple KNX lines, wire from the red and black terminals on
each gateway to the devices on the same KNX line.
-
Wire each KNX gateway to its own dedicated power supply on the KNX line. Do not
supply power to the gateway until after you turn on the network engine.
-
Go to Connecting the power source.